Add a Comment to a Ladder Diagram

When you are designing a Ladder Diagram, you can add comments that can be read by other users. You can use the comments to add any text, but typically they are used to explain the purpose of various parts of the Ladder Diagram.

To add a comment to a Ladder Diagram:

  1. Right-click on the background of the Ladder Diagram.
    A context sensitive menu is displayed.
  2. Select the Add Comment option to display the add comment window.

  3. Enter your comment.
  4. Select the OK button to confirm your entry and close the Add Comment window.
    The comment is added to the Ladder Diagram.

You can move the comment around on the Ladder Diagram in the same way as other items.

You can edit the comment by double-clicking on it—this will display the Edit Comment window which works in the same way as the Add Comment window.


Disclaimer

ClearSCADA 2017 R3