Add a Comment to a Sequential Function Chart

You can add comments to your Sequential Function Charts. The comments have no effect on the way an SFC works, but they can be used to provide information to other users. For example, you can add a comment that explains what happens when a certain action is performed.

To add a comment to an SFC:

  1. Display the SFC in Design mode (see Display a Sequential Function Chart).
  2. Right-click on the background of the SFC.
    A context sensitive menu is displayed.
  3. Select the Add Comment option.
    The Add Comment window is displayed.

  4. Enter the required comment. (Overwrite the default entry of <<comment>>).
  5. Select the OK button to confirm your entry and close the Add Comment window.
    The comment is added to the SFC. It will be visible to the users that access the SFC.

Disclaimer

ClearSCADA 2017 R3