CLOSE_FILE

Function Name

CLOSE_FILE

Description

Closes an open file or serial port. The CLOSE_FILE should be used after data has been written to a file or serial port.

Arguments

FILEID {UDINT}

The FILEID is a number that identifies the file or port that is to be closed.

For more information on the data types for the inputs and outputs, see Data Type Hierarchy.

Returns

Zero {UDINT}

The CLOSE_FILE function returns zero.

You should only use the CLOSE_FILE function in ST Programs.

Example:

ST Program - CLOSE_FILE:

To use a CLOSE_FILE function in an ST program, you need to use this syntax:

ClosePort := CLOSE_FILE(FILEID);

where ClosePort and FILEID are variables that are declared earlier in the ST program. The FILEID variable has to be a UDINT and identifies the file or port that is to be closed. The ClosePort variable is a UDINT and stores the zero that is returned by the CLOSE_FILE function.

For an example of the CLOSE_FILE function being used in an ST Program, refer to the example in WRITE_FILE.


Disclaimer

ClearSCADA 2017 R3