Comparison

You can use the COMPARISON functions to manipulate the flow of a program. For example, you can use an EQ function set a part of a program to be performed only if both of its input values are the same. This means that you can control whether the program, or parts of the program, run in different situations.

For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.


Disclaimer

ClearSCADA 2017 R3