Create a Sequential Function Chart Database Item
Each Sequential Function Chart needs to be represented in the ClearSCADA database by a Sequential Function Chart item. When you have created a Sequential Function Chart item, you can access its Edit feature which allows you to create the Sequential Function Chart program.
To create a Sequential Function Chart database item:
- Display the Database Bar (see Display an Explorer Bar).
- In the Database Bar, right-click on a system, Group, or Group Template to display a context sensitive menu.
- Select the Create New option, then the Logic option, then the Sequential Function Chart option from the context sensitive menu.
A new Sequential Function Chart item is added to the system, Group, or Group Template. It is selected automatically, ready for you to enter its name. - Enter a suitable name for the Sequential Function Chart then press the Enter key or select another part of the interface.
Now that you have created a Sequential Function Chart database item, you can display it and edit it as required.