Integer Formats

When you are specifying an integer value, either as a constant or as part of a variables definition, you need to specify the base. The base defines the type of value for the integer, and can be:


Disclaimer

ClearSCADA 2017 R3