LEN

Function Name

LEN

Description

Outputs the total number of characters in the input string.

Arguments

Input 1 {STRING}

The input is a string input.

For more information on the data types for the inputs and outputs, see Data Type Hierarchy.

Returns

Output {DINT}

The output is the total number of characters in the Input 1 string.

Example:

Function Block Diagram - LEN:

In this example, the input is 'PIPELINE STRUCTURE FAILURE' and so the LEN output is 26 (there are 26 characters in the input string).

ST Program - LEN:

To use a LEN function in an ST program, you need to use this syntax:

Output := LEN ('Input 1');

Where Output and Input 1 are defined as variables earlier in the ST program.


Disclaimer

ClearSCADA 2017 R3