SQRT

Function Name

SQRT

Description

Outputs the square root value of the input value. Both the input and output values are REAL or LREAL values.

Arguments

Input 1 {REAL or LREAL}.

For more information on the data types for the inputs and outputs, see Data Type Hierarchy.

Returns

Output {REAL or LREAL}

Example:

Function Block Diagram - SQRT:

In this example, the input of 5 is provided by the CurrentValue property of a point. The SQRT function outputs the square root of 5 which is 2.23606797749979.

ST Program - SQRT:

The syntax for an SQRT function in an ST Program is:

Output := SQRT (Input 1);

Where Output and Input 1 are defined as variables earlier in the ST program. The Input 1 variable represents a REAL or LREAL type of value (the output is the same type of value as Input 1).


Disclaimer

ClearSCADA 2017 R3