Configuring Lufkin SAMS Analog Input Points

With ClearSCADA’s Lufkin SAMS driver, you use:

You configure the properties of each Lufkin SAMS Analog Input point using fields on the Lufkin SAMS Analog Input Point Form.

This section covers configuration of properties on the Analog Point tab of the Lufkin SAMS Analog Input Point Form. For information on the fields on other tabs, see Tabs on Point Forms in the ClearSCADA Guide to Advanced Drivers.

For Lufkin SAMS Analog Input points, use the Analog Point tab to:


Disclaimer

ClearSCADA 2017 R3