Firmware Build Number

Associated with: Lufkin SAMS controllers

This status attribute indicates the build number of the firmware that is running in the controller. The attribute is displayed once the controller is or has been in communication with the server.

Also see Firmware Version.


Disclaimer

ClearSCADA 2017 R3