Specify the Dynacard Stores that Store the Rod Pump Data

Use these fields on the Lufkin SAMS tab to specify the ClearSCADA Dynacard Stores that store the rod pump readings:


With each of the above fields, select the browse button to display a Reference browse window. Select the required Dynacard Store from the window.

Further Information

Dynacard Stores in the ClearSCADA Guide to Advanced Drivers.


Disclaimer

ClearSCADA 2017 R3