Add a Button to a Mimic

You can add buttons to your Mimics. The buttons are rectangles that have a 3D appearance and can be animated so that when selected, they appear to be pressed down. By using the Animations feature, you can set a button to instigate a system action. For example, you can configure a button on a Mimic that, when selected, appears to be pressed down and causes a point to be overridden.

The buttons are designed to provide obvious interactive features on your Mimics.

Example:

To add a button to a Mimic:

  1. Display a Mimic in Design Mode.
  2. Select Button in the Drawing command group on the Graphics Tab.

  3. Draw the outline of the button by pressing the left-hand mouse button, and moving the cursor while keeping the left-hand mouse button pressed. The rectangle that is drawn is the space that will be occupied by the button.
  4. Release the left-hand mouse button to add the button.

When you have added the button, you can re-position it by selecting it and dragging it to a new location.

You can define the animations, pick actions and so on for the button by double-clicking on it to display its Properties window. For information on the button's property settings see Editing a Button.


Disclaimer

ClearSCADA 2017 R3