Alpha

The Alpha property represents the amount of transparency that is applied to the line/outline.

The Alpha property works in the same way as the FillAlpha property except that it animates the line/outline rather than the fill color. For more information, refer to the Fill Animations section (see FillAlpha).


Disclaimer

ClearSCADA 2017 R3