DashStyle

The DashStyle property defines the type of dashed lines that are used for a dashed line/outline.

Typically, you would set the DashStyle by defining the appearance of the dashes on the Line tab of the Polyline Properties window or the Text Properties window. However, you could use an expression to define the DashStyle or to animate the DashStyle according to the value or state of a database item.

Each DashStyle has a number that you can enter in an expression:

Number for Expression Style

0

Solid line

1

Dashed line

2

Dotted line

3

Dash-Dot line

4

Dash-Dot-Dot line

For example, you could animate the DashStyle so that it changes when a point has an unacknowledged uncleared alarm. The expression for this is:

LOOKUP( "<Path and name of point>.AlarmState" + 1, 0, 0, 0, 0, 4)

Where <path and name of point> is the location and name of the database point (do not enter the angle brackets < > ). AlarmState is the point property that affects the dashes and the numerical values are:

This means that the outline will be a solid line unless the point has an unacknowledged uncleared alarm.


Disclaimer

ClearSCADA 2017 R3