Design Considerations

We recommend that each Mimic you design is:

Parameter database items are different to Mimic parameters. Parameter database items store values that can be used to animate Mimic properties. Mimic parameters allow you to create embedded Mimics that vary according to the values associated with its parameters.

By taking these factors into account before you begin to design your Mimic, you can go on to create a Mimic that runs efficiently, and provides the functionality you require.

You should also consider:

When you have considered your design and are ready to begin the Mimic configuration, you will need to add objects to your Mimic (see Adding Objects to a Mimic), and you will need to edit them (see Mimic Editing Features).

Further Information

For more information on Group Templates, Group Instances, and Property Overrides, see Group Templates and Group Instances in the ClearSCADA Guide to Core Configuration.


Disclaimer

ClearSCADA 2017 R3