Editing an Embedded Image

When you have added an embedded image to a Mimic, you can access its Image Properties window to edit its settings. To display the window, double-click on the object on the Mimic. (For other ways of displaying the window, see Display the Properties Window for an Object on a Mimic.)

The Image Properties window contains a single tab—General.

The General tab contains Name, Visible, Animations, Pick Action, ToolTip, and Dynamic Position settings that work in the same way as on other General tabs (see General Tab). However, the General tab on the Image Properties window also contains Alignment settings:


Disclaimer

ClearSCADA 2017 R3