Removing a View

To remove a View that is no longer required:

  1. Display the Mimic that contains View that you want to remove. You need to display the Mimic in Design mode (see Displaying a Mimic).
  2. Select Views in the View command group on the Graphics Tab.

    The Views window will display.

  3. Select the View you want to edit from the Views list, then select the Remove button.

Only users with the Configure permission can remove Views.


Disclaimer

ClearSCADA 2017 R3