Rotating a Mimic Object

You can use the Rotate feature to rotate a Mimic object so that it is displayed at a different angle.

The Rotate feature is only available for Pipes, Lines, and Shapes.

To rotate a Mimic object:

  1. Display the relevant Mimic in Design mode.
  2. Right-click on the Mimic object that you want to rotate.
    A context sensitive menu is displayed.
  3. Select the Rotate option, then choose from:
    • Free—The object is selected for rotation. You control the amount of rotation by holding down the left-hand mouse button and using the mouse to move the cursor. Release the left-hand mouse button when the Mimic object is shown at the required angle.
    • 180—Rotates the object by 180°.
    • +90—Rotates the object 90° clockwise.
    • +60—Rotates the object 60° clockwise.
    • +45—Rotates the object 45° clockwise.
    • +30—Rotates the object 30° clockwise.
    • -30—Rotates the object 30° anti-clockwise.
    • -45—Rotates the object 45° anti-clockwise.
    • -60—Rotates the object 60° anti-clockwise.
    • -90—Rotates the object 90° anti-clockwise.

You can also access the Rotate options via the Orientation command in the Arrange group on theGraphics Tab.

For information on setting up a rotation animation, see Rotation Animations.


Disclaimer

ClearSCADA 2017 R3