Use a Go To link on a Form to Display a Mimic

If you are logged on via a User account that can access configuration Forms for database items, you can use a Go To link to display a Mimic. This is only applicable when the Mimic you want to display has been associated with an item via a configuration field. For example, if the Mimic has been set as the Help View for database point, you can display the Mimic by selecting the Go To link next to the Help View field on the point’s Form.


Disclaimer

ClearSCADA 2017 R3