Use an Alarms List or Alarm Banner to Display a Mimic

If an alarm is raised for a database item, and that item is configured to have an Alarm View or Help View, you can use the Display Alarm View and Display Help View actions to display a Mimic. Simply right-click on the relevant alarm in the Alarms List or Alarm Banner, then select:

The Alarm Banner is only available in ViewX.

Further Information

Alarm Banner: see Alarm Banner in the ClearSCADA Guide to Alarms.

Alarms List: see Alarms Lists in the ClearSCADA Guide to Alarms.


Disclaimer

ClearSCADA 2017 R3