Using Embedded Objects on Mimics

Mimics can contain embedded objects such as Trends, Lists, and other Mimics. Each embedded object provides access to the same features as the original version.

Example:

A Mimic named 'River Level and Flow' contains several control buttons. When selected, these buttons allow the user to override points.

The 'River Level and Flow' Mimic is embedded on another Mimic named 'Overview'. Users can select the control buttons on the embedded version of the 'River Level and Flow' Mimic in the same way as if the users had selected the buttons on the original 'River Level and Flow' Mimic.


Disclaimer

ClearSCADA 2017 R3