The Transmission Control Protocol Supported by ClearSCADA

Each MELSEC A PLC can use one of four Transmission Control Protocol formats to communicate with its Mitsubishi Master, via RS-232.

ClearSCADA communicates with MELSEC A PLCs using Transmission Control Protocol Format 1.

For ClearSCADA to communicate with MELSEC A PLCs, set the Mode Setting switch on each PLC to indicate Protocol 1 (typically switch setting 1).

For more information, see the Mitsubishi documentation supplied with MELSEC A PLCs.


Disclaimer

ClearSCADA 2017 R3