Modbus Exception Errors

A remote Modbus device might return an exception error for various reasons. Should an exception occur, ClearSCADA will set the affected Modbus scanner to ‘Failed’. The alarm that is raised will indicate the reason for the failure. With the Simple Modbus driver, an exception might be generated if any of the following occur:

A Modbus scanner’s Comms Statistics status attribute indicates if any exception errors have occurred since that scanner was last restarted.


Disclaimer

ClearSCADA 2017 R3