Which Driver?

ClearSCADA is able to communicate with Modbus devices using one of several ClearSCADA drivers. Which driver you use depends on your system set-up and configuration requirements. This section briefly summarizes the different options that are available.

The drivers that you can use to communicate with Modbus devices include:

Further Information

Supported Drivers and Protocols.


Disclaimer

ClearSCADA 2017 R3