Configure the NTP Monitor Point Properties

Use the fields on the NTP Monitor tab of each NTP Monitor <Point Type> Form to configure these properties:


The NTP Monitor tab on the NTP Monitor Analog Point Form also includes this field:


Disclaimer

ClearSCADA 2017 R3