Configure SQL Query Lookup Properties

Use these fields on the ODBC tab to specify general and SQL Query Lookup properties of a point. The fields at the top of the tab are common to points on many simple drivers (see Configure Common Point Properties in the ClearSCADA Guide to Simple Drivers).

Fields that are specific to the ODBC driver are explained below:


Disclaimer

ClearSCADA 2017 R3