Configure the Query Properties

Use the fields on the Query tab to define the request for data transfer, how often that request is sent to the other application, and the connection used to access that application:

Each Query is executed on system or driver start-up, and thereafter at the specified Scan Rate interval, or whenever a Refresh is requested (for example, by an operator selecting the Refresh pick action for a Query).

Whenever a Query is executed, the data that is sent to ClearSCADA as a result of that query is stored in a results table, internally within the ODBC driver. You then use ODBC points (see Points Used for ODBC Data Transfer) to extract particular data values from that table.


Disclaimer

ClearSCADA 2017 R3