Configure Common Point Properties on the OPC XML-DA Tab

Use the fields at the top of the OPC XML-DA tab to configure the general point properties of each point. Some of these fields are common to many simple drivers (see Configure Common Point Properties in the ClearSCADA Guide to Simple Drivers). Fields that are specific to points on the OPC XML-DA Client driver are explained below:


Disclaimer

ClearSCADA 2017 R3