Which Driver?

ClearSCADA is able to read and/or write to data on other servers using one of two OPC standards: OPC DA, and OPC XML-DA. Whether you choose to use the ClearSCADA Advanced OPC Driver, the ClearSCADA Simple OPC Driver, or the ClearSCADA OPC XML-DA Driver, depends to some extent on your system setup. OPC DA is more efficient in terms of network bandwidth than OPC XML-DA. However, OPC DA is based on DCOM and can be difficult to set up when the driver and target OPC DA server are on opposite sides of a firewall. OPC XML-DA uses standard web protocol and is much more firewall friendly.

To choose the right driver for your requirements, you need to consider whether you place more significance on efficient use of network bandwidth or ease of setup:


Disclaimer

ClearSCADA 2017 R3