Display the WebX Interface

ATTENTION: This topic relates to the deprecated Original WebX client that is supported by this and previous versions of ClearSCADA. For information about the WebX client that is supported by ClearSCADA 2015 R1 onwards, for which the web server is hosted using IIS, click here.

To display the WebX interface:

  1. Run Internet Explorer.
  2. To display the WebX interface from a ClearSCADA server, enter http://localhost in the Address field.

    To display the WebX interface from a client, enter the server name in the Address field.

  3. Press the Enter key. This displays the WebX home page.

    If the WebX home page is not displayed, there may be a certificate error. You may need to use an alternative address or port number. For more information, see Run a WebX Client in the ClearSCADA Guide to ViewX and WebX Clients.

The WebX home page contains a navigation bar featuring the following buttons:

When you have displayed the WebX home page, proceed to Log on to the System via WebX.

Further Information

Understanding WebX: see WebX Client in the ClearSCADA Guide to ViewX and WebX Clients.


Disclaimer

ClearSCADA 2017 R3