Configuring Pager Server Settings

The ClearSCADA server has 1 Pager Driver-specific setting that you may need to configure:

Typically, you would only need to consider adjusting this setting if there are alarms on your system relating to multipage messages not being delivered in full. Normally this type of alarm indicates that there is an unexpected problem with the communications network as the messages are not being sent within the expected amount of time. However, it is possible that a low Multipage SMS Message Timeout setting could also cause the multipage messages to be disregarded (by not allowing enough time for each page of the messages to arrive).

For information on the Multipage SMS Message Timeout, see Define Multipage Message Settings.


Disclaimer

ClearSCADA 2017 R3