Define the Content of a Pager Message

When sending a message from ClearSCADA to a pager device or mobile telephone, you need to use the Send Message or Send Pager Message window to define the content of your message:

  1. Display the Send Message or Send Pager Message window by right-clicking on a Pager Service or User and selecting the Send Message or Send Pager Message action (see Sending a Message Manually).
  2. Enter the characters that comprise your message in the Message field. The message that you enter will be the message that is displayed on the recipient pager device or mobile telephone.

    Your message will be shortened if it exceeds the Maximum Message Length that has been configured for the Pager Service used to send the message. The method that ClearSCADA uses to shorten the message is also defined in the Pager Service configuration. For more information, please refer to Define the Maximum Message Length Properties for a Pager Service.

Further Information

Sending a Message Manually.


Disclaimer

ClearSCADA 2017 R3