View your QueryPad Command History

Within the SQL Entry pane you can use CTRL+ the Up or Down arrow keys to view the commands you have made (in sequential order). This is useful when you have used QueryPad to display a significant amount of information, as it allows you to quickly find previous commands so that you can retreat them or make further commands that are similar.

To view the command history, you have to be logged on to QueryPad and have made one or more commands.

To view the command history:


Disclaimer

ClearSCADA 2017 R3