How can I read the gas composition for a specific run?

The ROC PlusDemo.sde file includes demonstrations of how to read the gas composition for a run.

In summary, you will need to set up a ROC Plus Numeric Point for each parameter that you want to read and then configure that point with the appropriate TLP. For example, the Type and Parameter for nitrogen is 112 and 26. The run number will determine the Location value.


Disclaimer

ClearSCADA 2017 R3