Primary Connection Tab - Serial Connection

Display the Properties window (‘configuration Form’) for a ROC Plus Channel object and then select the Primary Connection tab. If your channel uses serial communications, set the Connection Type to Serial. The tab contains the standard serial connection options, such as baud rate, parity and so on. These settings need to match the settings in the ROC.


Disclaimer

ClearSCADA 2017 R3