Alarm Limits

Use the fields within the Alarm Limits section of the Analog Point tab to set alarm limits for a point and to specify whether ClearSCADA generates an alarm or event if the point exceeds those limits.

Some of the Alarm Limits fields are common to many analog points (see Configure the Limits for an Analog Point in the ClearSCADA Guide to Core Point Configuration).


Disclaimer

ClearSCADA 2017 R3