Configuration Field

Associated with: SCADAPack 50 Outstations.

This status attribute shows a device point and a device field affected by a configuration download from ClearSCADA. It indicates that a user has sent a change from ClearSCADA to the device. It does not imply that the device has received and processed the change. This is indicated by the device sending a confirmation SMS message back to ClearSCADA.

The attribute format is as follows:

Point <device point name> :<field name>.

Example:

Point V1 : Var Name.

For more information, see Number of Outstanding SMS Requests.


Disclaimer

ClearSCADA 2017 R3