Device Point Mapping

Associated with: SCADAPack 50 Points and SCADAPack 50 Outstations.

For points, this status attribute shows the device point (V1-V8) to which a ClearSCADA point maps, as shown in the illustration below:

You use this status attribute in conjunction with the Device Point - Number of Confirmed Changes and the Device Point - Number of Unconfirmed Changes status attributes.

 

For outstations, the Status display shows this information for each device point that is mapped to a ClearSCADA point. There is one Device Point Mapping attribute line for every mapped point, as shown in the illustration below:

 

When you make a change to a device point's mapping in ClearSCADA, ClearSCADA will display a Device Point Mapping message in the Outstation Status window. An example is shown in the illustration below:

 

For more about mapping device points, see Map ClearSCADA Points to SCADAPack 50 Device Logical Points.


Disclaimer

ClearSCADA 2017 R3