Expires

Associated with: SCADAPack 50 Outstations.

This status attribute shows the date and time by which a confirmation response, sent by the device, needs to be received by ClearSCADA to be valid. After this time, ClearSCADA will flag the confirmation response as unexpected, although it will process the confirmation. There can be significant delays in sending and receiving SMS messages, even when ClearSCADA and the device are operating normally. This is because the GSM network may be busy or the device may be in Sleep mode.

Further Information

For more information about outstanding confirmation messages, see Number of Outstanding SMS Requests.

For more information about how ClearSCADA communicates with the SCADAPack 50 device by using SMS messages, see SCADAPack 50 and SMS Messaging.


Disclaimer

ClearSCADA 2017 R3