Specify an Outstation Name

Use the Outstation Name field on the SCADAPack 50 tab to specify a device name. ClearSCADA can potentially receive messages from many devices. The Telephone Number and Outstation Name together identify to ClearSCADA which device this is (see Specify an Outstation Telephone Number).


Disclaimer

ClearSCADA 2017 R3