Configure the General SCADAPack Modbus Analog Point Properties

For information on configuring properties on SCADAPack Modbus analog points other than SCADAPack Modbus Analog Input Points and SCADAPack Modbus Analog Output Points, see theSCADAPack Modbus Realflo driver extension guide.

Use the fields at the top of the Analog Point tab on the SCADAPack Modbus Analog Point Form to Configure Common Point Properties. Fields that are specific to SCADAPack Modbus Analog points are explained below.


Disclaimer

ClearSCADA 2017 R3