IO Controller Firmware Version

Associated with: SCADAPack controllers

This attribute indicates the version of I/O firmware that is running on a controller. The attribute is displayed once a controller is or has been in communication with the server.

Example:

3


Disclaimer

ClearSCADA 2017 R3