Version Number

Associated with: SCADAPack controllers

This attribute indicates the version number of the firmware that is running on the controller. The attribute is displayed once a controller is or has been in communication with the server.

Example:

2.11
(for a controller that is running firmware version 2.11)


Disclaimer

ClearSCADA 2017 R3