Configuring Realflo Analog Input Points

SCADAPack Realflo controllers support ‘standard’ SCADAPack Modbus Analog Input points and Analog Output points (see Points Used on SCADAPack Modbus Realflo Controllers). SCADAPack Modbus Realflo controllers also support SCADAPack Modbus Realflo Analog Input points—points that are used to process flow calculation data in ClearSCADA (see Configure ClearSCADA to Monitor Realflo Calculation Data).

Many items of Flow Run data are available directly from the Flow Run itself—to enable users to view such data, you can attach the Flow Run properties to a display, such as a Mimic, or a Trend. (In such cases, you only need to associate the data with an analog point if you want ClearSCADA to further process or store the Flow Run data—for more information, see View and Process Flow Run Data.)

Some items of Flow Run data are not available directly from the Flow Run database item—they are calculated using the Flow Run’s configuration, but are stored internally. To view or process these items of data in ClearSCADA, you have to configure one SCADAPack Modbus Realflo Analog Input point per item of data to which you require access.

This section summarizes the Realflo-specific properties that apply to SCADAPack Modbus Realflo Analog Input points. You configure these properties using the fields on the Analog Point tab of the SCADAPack Modbus Realflo Analog Input Point Form.

Use the Analog Point tab to:

The fields on other tabs are common to points on many advanced drivers (see Tabs on Point Forms in the ClearSCADA Guide to Advanced Drivers).


Disclaimer

ClearSCADA 2017 R3