Forced Static Pressure

Associated with: Flow runs

To enable a Gas Flow Computer to continue to calculate gas flow data while any of its sensors are being calibrated, a Flow Run can be configured to use ‘forced’ values in its calculations. Once the sensors are calibrated, the flow calculations revert to using live values and the forced values are disabled.

This attribute indicates the forced static pressure that is presently being used in the Flow Run’s flow calculations. The attribute is displayed once the server has retrieved Flow Run data from a Realflo-enabled SCADAPack controller. The units that apply to the attribute depend on the Measurement Units system being used for the Flow Run’s Contract Units.

Example:

15.1657
(for a value in KPa)


Disclaimer

ClearSCADA 2017 R3