Introduction to the SCADAPack Modbus Realflo Driver

This driver is an extension driver. It provides additional application-specific functionality to the 'parent' driver with which it is associated. To interact successfully with devices using an extension driver, you need to:

Intended Audience

This guide is primarily intended for engineers who are responsible for configuring ClearSCADA to interface with Realflo.

The guide also contains information for:

Document Scope

This guide explains the configuration, features and database items that are specific to ClearSCADA's SCADAPack Modbus Realflo driver. The SCADAPack Modbus Realflo driver is a SCADAPack Modbus extension driver. It provides additional functionality to enable ClearSCADA to interface with SCADAPack controllers that are running Realflo. The Realflo feature converts a SCADAPack controller into an electronic Flow Computer. ClearSCADA can interface with Realflo, in order to monitor and process the gas, liquid or water flow data that is being retrieved by the Flow Computer. ClearSCADA can access the Flow Computer’s data, configuration and calculation factors by interrogating the Realflo components on the SCADAPack controllers. When ClearSCADA interacts with a controller’s Realflo components, the SCADAPack controller is referred to as a Realflo controller throughout the ClearSCADA documentation, to indicate that additional interaction.

In order to communicate with Realflo controllers, your ClearSCADA system needs to be running the following drivers:

If required, ClearSCADA can export retrieved flow measurement data in Common File Exchange (CFX) format. The CFX file format is proprietary and confidential to Flow-Cal, Inc. The exported data can then be imported into any of Flow-Cal’s measurement data management applications. To export data in this format, ClearSCADA also needs to be running the CFX driver. For information on that driver, see the ClearSCADA Guide to the CFX Export Driver.

Use this ClearSCADA Guide to the SCADAPack Modbus Realflo Driver alongside the ClearSCADA Guide to the SCADAPack Modbus Driver and the ClearSCADA Guide to the Advanced Modbus Driver. As much of the information in the latter guides is assumed knowledge, we recommend that you read the guides mentioned above before reading this driver guide.

The SCADAPack Modbus Realflo driver documentation:

In addition it explains features that are of interest to operators, such as:

Driver-specific aspects that are of interest to system administrators and engineers when investigating unexpected behavior relating to the SCADAPack Modbus Realflo driver. For information, see:

Further Information

For further information on Realflo, or on gas, liquid or water flow data that is not covered by this guide, please refer to the documentation provided with the Realflo application.

Realflo Flow Computer functionality is licensed by Schneider Electric TRSS. For more information, see the Schneider Electric TRSS website.


Disclaimer

ClearSCADA 2017 R3