Read Configuration

Associated with: SCADAPack Modbus Flow Runs

Security permission required to access this pick action: Configure

NOTICE

UNEXPECTED BEHAVIOR OF APPLICATION

Use the Read Configuration action with care. The action will overwrite the configuration on a Flow Run’s Flow Run, Compressibility Calculation, and Flow Calculation tabs, other than the Basic Flow Run properties and the Scanning properties (both configured on the Flow Run tab).
Failure to follow these instructions can result in unexpected configuration changes.

When a Flow Run is added to the ClearSCADA database, basic settings, such as the controller with which the Flow Run is associated, have to be specified on the Flow Run Form (see Preparation and Minimum Configuration). You can then either specify the rest of a Flow Run’s configuration in ClearSCADA , or have the driver read (‘upload’) the majority of an existing Flow Run’s configuration from the controller into ClearSCADA(see Configure or Read the Flow Run Configuration).

In order to read the configuration from an existing Flow Run into ClearSCADA :

If you specify that ClearSCADA is to read the majority of a Flow Run’s configuration from a controller, ClearSCADA will automatically scan the Realflo controller for Flow Run configuration, at the frequency specified in the Scanning section of the Flow Run Form (see Configure the Scanning Properties). This Flow Run Configuration Scan is a ‘fall back’ measure, to confirm that a Flow Run’s configuration data remains up to date in the ClearSCADA database. Should a read occur while a Flow Run’s configuration Form is open and an attempt be made to save any user-instigated configuration changes to that Flow Run after the read is complete, a diagnostic message will be displayed. The message will indicate that the Flow Run’s configuration has changed on the server since the Form was opened. Options are provided to discard the user-instigated changes or overwrite the server’s Flow Run configuration with those changes.

If changes are made to such a Flow Run’s configuration and the next scheduled Flow Run Configuration Scan is not imminent, use the Read Configuration pick action to read that configuration into ClearSCADA .


Disclaimer

ClearSCADA 2017 R3