Reset Sensor Statistics
Associated with: SCADAPack Modbus Flow Runs
Security permission required to access this pick action: Diagnostics
This pick action is supported by Realflo 6.90 onwards.
Use the pick action to reset the sensor statistics and/or Coriolis meter statistics on a Flow Run.
Select the pick action to display the Reset Sensor Statistics window.
Use the window's check boxes to specify the statistics that ClearSCADA is to reset.
- Reset Sensor Statistics—Select this check box to reset the sensor statistics.
Clear the check box if you do not want to reset the sensor statistics.
- Reset Coriolis Meter Statistics—Select this check box to resent the Coriolis meter statistics.
Clear the check box if you do not want to reset the Coriolis meter statistics.