Source (Gas Flow Run)

Associated with: SCADAPack Modbus Realflo Outsations, and SCADAPack Modbus Realflo Analog Input points

The Source attribute is common to many Status displays. The attribute indicates the location at which an item resides. The information shown varies, depending on the type of item.

For SCADAPack Modbus Realflo Outstations, the attribute displays information in this format:

Set <Set Address>:OS <Controller Address>

For SCADAPack Modbus Realflo Analog Inputs, the attribute displays information in this format:

Set <Set Address>:OS <Controller Address>:Flow Run <Flow Run Number>:AI Source <Source Number>:Item <Item Number> (Address <Point Address>)

where:

For information about either of the above properties, see Configure the General Realflo Analog Point Properties.

The table below indicates the type of Flow Run Source <Source Number > represents.

Source Number Source Type
0 Accumulation
1 Input
2 Flow Calculation
3 Compressibility Calculation
4 Density Calculation
10 Daily Flow History
11 Hourly History Data
12 Batch Records Data

The table below indicates the type of Flow Run Data Item <Item Number > represents, when the Source Type for the Analog Input Point is defined as Accumulation (<Source Number>=0).

Item Number Gas Flow Run Data Item Type
1 Uncorrected flow volume during previous month (AGA-7 Only)
2 Uncorrected flow volume during current month (AGA-7 Only)
3 Uncorrected flow volume during previous contract day (AGA-7 Only)
4 Uncorrected flow volume during current contract day (AGA-7 Only)
5 Number of flow calculations during contract day
6 Duration of flow during contract day
7 Flow volume at base conditions during contract day (gas only)
8 Flow mass at base conditions during contract day (gas only)
9 Flow energy at base conditions during contract day (gas only)
10 Total accumulated flow volume at base conditions (gas only)
11 Flow duration in current month
12 Flow volume in current month
13 Flow duration in previous month
14 Flow volume in previous month
15 Duration of flow during previous contract day
16 Flow volume at base conditions during previous contract day
17 Flow mass at base conditions during previous contract day
18 Flow energy at base conditions during the previous contract day
19 Number of flow calculations during previous contract day

The table below indicates the type of Flow Run Data Item <Item Number > represents, when the Source Type for the Analog Input Point is defined as Input (<Source Number>=1).

Item Number Gas Flow Run Data Item Type
1 Calibration flags
2 Temperature Input Alarm
3 Static Pressure Input Alarm
4 Differential Pressure (AGA-3 and V-Cone only) input Alarm
4 Turbine Pulses (AGA-7 only) input Alarm
4 Mass Flow (AGA-11//Liquid/Water) Input Alarm
4 Mass Pulse (AGA-11//Liquid/Water) Input Alarm
5 Live turbine meter pulses (AGA-7 or Mass/Volume Pulse AGA-11/Liquid/Water)
6 Live Temperature
7 Live Static Pressure
8 Live Differential pressure (AGA-3 and V-Cone only)
8 Live Mass Flow (AGA-11/Liquid/Water)
9 Forced Temperature
10 Forced Static Pressure
11 Forced Differential Pressure (AGA-3 and V-Cone only)
11 Forced Mass Flow (AGA-11/Liquid/Water)
12 Forced Pulse Rate (AGA-7 or Mass/Volume Pulse AGA-11/Liquid/Water)
13 Current turbine meter pulses (AGA-7 Gas or Mass/Volume Pulse AGA-11/Liquid/Water)
14 Current Differential Pressure (AGA-3 and V-Cone only)
14 Current Mass Flow (AGA-11/Liquid/Water)
15 Current Density
16 Current Water Cut
17 Current Input Temperature
18 Current Static Pressure
19 Density Input Alarm
20 Water Cut Input Alarm
21 Live Density
22 Live Water Cut
23 Forced Density
24 Forced Water Cut

The table below indicates the type of Flow Run Data Item <Item Number > represents, when the Source Type for the Analog Input Point is defined as Flow Calculation (<Source Number>=2).

Item Number Gas Flow Run Data Item Type
1 Compressibility approximated flag
2 Input or flow calculation error code
3 Flow volume rate
4 Flow mass rate
5 Flow energy rate (gas only)
6 Flow extension (AGA-3 1992/2013 only)
6 Flow product (AGA-3 1985 only)
6 Uncorrected flow volume (AGA-7 only)
7 Date of Flow Update
8 Time of Flow Update

The table below indicates the type of Flow Run Data Item <Item Number > represents, when the Source Type for the Analog Input Point is defined as Compressibility Calculation (<Source Number>=3).

Item Number Gas Flow Run Data Item Type
1 Compressibility calculation result code
2 Supercompressibility
3 Real relative gas density
4 Mass density at flow conditions
5 Mass density at base conditions
6 Date of Compressibility Update
7 Time of Compressibility Update

The table below indicates the type of Flow Run Data Item <Item Number > represents, when the Source Type for the Analog Input Point is defined as Density Calculation (<Source Number>=4).

Item Number Gas Flow Run Data Item Type
1 Heating value

The table below indicates the type of Flow Run Data Item <Item Number > represents, when the Source Type for the Analog Input Point is defined as Daily Flow History (<Source Number>=10), or Hourly History Data (<Source Number>=11).

Item Number Gas Flow Run Data Item Type
1 Duration of flow in period
2 Flow volume at base conditions
3 Flow mass at base conditions
4 Flow energy at base conditions
5 Flow extension (AGA-3 1992/2013 only)
5 Flow product (AGA-3 1985 only)
5 Uncorrected flow volume (AGA-7 only)
5 Integral value (AGA-11 Only)
6 Average temperature
7 Average static pressure
8 Average differential pressure (AGA-3 and V-Cone only)
8 Average Mass Flow (AGA-11 Mass Flow Only)
9 Average number of rotations per second (AGA-7 and AGA-11 Mass Pulse only)
10 Average real relative gas density
11 Input Units
12 Contract Units
13 Number of Alarms
14 Number of Events
26 Batch ID
27 Duration of period
28 QTR Identifier

The table below indicates the type of Flow Run Data Item <Item Number > represents, when the Source Type for the Analog Input Point is defined as Batch Records (<Source Number>=12).

Item Number Gas Flow Run Data Item Type
1 Flow Time
2 Flow volume at base conditions
3 Flow mass at base conditions
4 Flow energy at base conditions
5 Uncorrected flow volume (AGA-7 only)
5 Flow extension (AGA-3 1992/2013 only)
5 Flow product (AGA-3 1985 only)
5 Integral Value (AGA-11 Only)
6 Average Temperature
7 Average Pressure
8 Average differential pressure (AGA-3 and V-Cone only)
8 Average Mass Flow (AGA-11 Mass Flow Only)
9 Average number of rotations per second (AGA-7 and AGA-11 Mass Pulse only)
10 Average real relative gas density
11 Input Units
12 Contract Units
13 Alarm Count
14 Event Count
26 Batch ID
27 Duration of period
28 QTR Identifier

Disclaimer

ClearSCADA 2017 R3