Static Pressure Properties

The fields within this section of the Flow Run tab display those properties that are associated with Static Pressure measurement.

You can configure these properties directly in ClearSCADA, or read the configuration into the ClearSCADA database (see Configure or Read the Flow Run Configuration).

Use the input alarms section of the Static Pressure section to set the alarm thresholds for alarm types that have been enabled in the Input Properties section.

Use the following properties to configure alarm limits in the Static Pressure section:

Further Information

For more detailed information on these properties, see the documentation provided with the Realflo application.


Disclaimer

ClearSCADA 2017 R3